Port Server on Remote Computer for Remote Access to Serial Ports

You can install the port server software on a remote computer to allow the Geo SCADA Expert servers to access any devices that are connected to the remote computer's serial port(s). The remote computer can provide connections to multiple servers (and external applications) as well as the serial connection to outstations or other devices.

The remote computer has TCP/IP network connection to the Geo SCADA Expert servers. It also has serial connections to the outstations that monitor and control plant.

The Geo SCADA Expert servers can communicate with the outstations via the remote computer. The servers communicate with the remote computer via a TCP/IP connection. The remote computer then communicates with the outstations that are connected to the serial port.

Data received by the port server via the TCP/IP network is transmitted to the outstations via the assigned serial port. Similarly, data received via the assigned serial port is transmitted to the server via the TCP/IP network. Both statically assigned ports and dynamically assigned ports can provide remote access to serial ports.

One of the uses for remote access to serial ports is to provide each server in a multi-server system access to the same devices. This type of communications setup is required as a serial connection is point-point—it only allows for a single connection, whereas multiple connections are needed due to there being multiple Geo SCADA Expert servers (and possibly other external applications).

Any serial port on the remote computer can be assigned when requested by
a Geo SCADA Expert server (this is referred to as a dynamically assigned port) or can be assigned by the port server as soon as it starts (this is referred to as a statically assigned port). The type of port you need is dependent on your requirements:


Disclaimer

Geo SCADA Expert 2019