Client PC Requirements

When purchasing clients for use with Geo SCADA Expert, there are many factors you need to consider, including the operating systems supported by Geo SCADA Expert and the type of displays required.

In the following sections, we describe the recommended specifications for clients that are to use Geo SCADA Expert:

You should also refer to the following sections, which apply to both Geo SCADA Expert servers and Geo SCADA Expert clients:


Disclaimer

Geo SCADA Expert 2019