Configuring TBox Digital Points

The TBox driver supports 1-, 2-, and 3-bit Digital Input points and Digital Output points.

Configure the properties for each digital point using the fields on the TBox Digital Input Point Form or the TBox Digital Output Point Form, as appropriate.

Use the Digital Point tab to:

For TBox Digital Output Points only, there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to specify properties relating to control of equipment:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).


Disclaimer

Geo SCADA Expert 2019