Channel Configuration

Totalflow channels are used to provide Geo SCADA Expert with additional connection information, so that the server can successfully communicate with Totalflow devices.

Specify the features for each channel by using the fields on the Totalflow Channel Form.

The Form has several tabs. This section explains the driver-specific fields on the:

For information on common fields on these tabs, see Configuring Channels on Simple Drivers in the Geo SCADA Expert Guide to Simple Drivers.

For information on the fields on other tabs, see Tabs That are Common to Many Configuration Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2019