Scanners Group

The example project includes a Scanners group.

The Scanners group contains the Totalflow Scanner items that connect the Point items to the Channel items.

A Totalflow Scanner can only have one sampling interval and one offset. The example database includes multiple scanners, each with their own polling rate. They are set up as follows:

Using a single scanner on a Totalflow device would be acceptable, providing that only one sampling interval and offset were required.

Further Information

Scanner Configuration

Totalflow Channel

Totalflow Numeric Point

Totalflow Digital Point

Totalflow History Point

Totalflow String Point


Disclaimer

Geo SCADA Expert 2019