Installing the In-Database Translation Dictionary Excel Add-In Program

The In-Database Translation Dictionary is part of the Geo SCADA Expert database and, for convenience, you can create and maintain it in a Microsoft® Excel® spreadsheet by using an Excel add-in program.

You can install the Excel add-in program on any server or client computer that meets the following recommended specifications:

You should also have Excel installed on the computer.

You can install the Excel add-in program from either:

 

To install the add-in program from the Geo SCADA Expert Resource Center:

  1. In the ViewX client, select the File menu.
    A context-sensitive menu is displayed.
  2. Select the Help option.
    A further context-sensitive menu is displayed.

  3. Select the Online Resource Center option.

    The Resource Center Home screen is displayed.

  4. Select the Install Geo SCADA Expert Excel Dictionary Tool option.

    The Excel add-in program Setup Wizard displays.

  5. Follow the displayed instructions to install the add-in program.

 

To install the add-in program from the Geo SCADA Expert installation CD or DVD:

  1. Insert the Geo SCADA Expert CD. If Autorun is disabled on your PC, run the CD manually.
  2. When the Installer screen is displayed, select Install Geo SCADA Expert Excel Dictionary Tool.

    The Excel add-in program Setup Wizard displays.

  3. Follow the displayed instructions to install the add-in program.

Disclaimer

Geo SCADA Expert 2019