Hand Control

Associated with: Internal Points

Security permission required to access this option: Control

Use this option on the Object Menu to manually change an internal point’s value.

Select the Hand Control option to display the Hand Control window.

Specify the required value in the Value field:

Select the OK button to confirm the entry and hand control the point.

If using this pick action with the Automation Interface, you need to specify the method name CurrentState for a digital point, or CurrentValue for other types of point.


Disclaimer

Geo SCADA Expert 2019