Trends

Trends are graphical displays that plot the values of database items. They allow you to view and compare the values of points over a specific period of time.


Trends display data with the x-axis representing time, and the y-axis representing data values. Trends can be configured to display multiple traces simultaneously.

Geo SCADA Expert supports several types of Trend:

Higher level users can also access Ad Hoc Trends for specific items or properties from the OPC Data Bar or OPC Historic Data Bar. For more information, see Working with the OPC Data Bar, and see Working with the OPC Historic Data Bar.

For more information on using Trends, see the Geo SCADA Expert Guide to Trends.

Geo SCADA Expert also supports special types of Trends, such as X-Y Plots, and X-Y-Z Plots. For more information, see the Geo SCADA Expert Guide to X-Y Plots, and the Geo SCADA Expert Guide to X-Y-Z Plots.


Disclaimer

Geo SCADA Expert 2019