Understanding Your System
You can use ViewX (the primary Geo SCADA Expert Man-Machine Interface)
To learn about the basic concepts of a Geo SCADA Expert system, see these sections:
For further information on the types of Geo SCADA Expert client you might use, see ViewX Client
For information on the types of driver that might be installed on your system, and for an overview of master-slave setups, and direct and PSTN communications, see Welcome to the Geo SCADA Expert Guide to Drivers.
For information on the terminology used throughout this guide, see Terminology.