Choosing a Configuration Strategy for WITS

When configuring a new Field Device, you need to choose an appropriate configuration strategy. To choose a strategy, you need to consider:

Taking the above considerations into account, you need to make some decisions:

Are you going to use Group Templates? If yes, see Using Group Templates with WITS Field Devices.

Are you going to use a vendor-supplied tool, such as the Configuration Application to apply most of the incremental configuration? If yes, use one of the following strategies:

Are you going to use Geo SCADA Expert to apply most of the incremental configuration? If yes, use one of the following strategies:

You may also decide that you want to pre-configure Geo SCADA Expert and then upload or import the configuration at a later time. If so, see Pre-Configure Geo SCADA Expert - Upload or Import Later.

If you want to make configuration changes to WITS Field Devices that have already been set up to work with Geo SCADA Expert, see Making Changes to WITS Field Device Configuration


Disclaimer

Geo SCADA Expert 2019