Inhibit Alarms/Events (WITS Point)

Associated with: WITS Database Points

Security permission required to access this pick action: Disable Alarms

You can use Inhibit Alarms/Events to restrict the Field Device so that it does not report DNP3 events and/or logging events for a point. However, an inhibit does not prevent the periodic logging of values for the point or the reporting of its current statuses or current values. Inhibits are useful when you know that a point is going to generate unnecessary events, for example, if a measuring instrument has developed a fault.

An inhibit on an individual point is separate to an inhibit on all points (inhibit applied the WITS Outstation). For example, you could inhibit an individual point and then inhibit the WITS Outstation (with which the point is associated). If you then remove the inhibit on the WITS Outstation, the individual point will remain inhibited.

When you select Inhibit Alarms/Events, you can choose from:

If supported by your Field Device, you can also define a Timeout for the inhibit. The Timeout is an OPC time interval, in seconds (see OPC Time Format). If you enter 0, no Timeout is used. If you specify a Timeout, the inhibit will remain in place until:

If a Timeout is not used (or not supported) the inhibit applies until:

The View Status window for the Point shows the current inhibit status.


Disclaimer

Geo SCADA Expert 2019