Severity Types and Actions for WITS Database Points

Each point state has a Severity type that defines whether Geo SCADA Expert logs an event or raises an alarm when the point changes state (see Define the Severity Type). For WITS database points, the Severity types also define the action taken by the Field Device when the point changes state.

When a WITS Field Device performs an action, it generates or logs an event, and may initiate a connection to Geo SCADA Expert. There are two types of event:

Log events are WITS-specific and are treated in the same way as other events in Geo SCADA Expert (see Events Clients).

When you configure a WITS point, you can define the action Severity for each alarm limit, state, and DNP3 Object Flag. The Severity and action settings are shown on the Point Form (on the tab for the type of point, for example, the Analog Point tab for a WITS Analog Input point).

Severities for Alarm Limits - WITS Analog Point Form

Point States

Form Geo SCADA Expert Field Device
None No Action Taken No Action Taken
Log Event Log State Change Event in Event Journal Log State Change Event in Data Log
Event Log State Change Event in Event Journal Generate DNP3 Event
Alarm Raise Alarm Generate DNP3 Event and Open Connection

Fleeting

(On binary points)

Raise Fleeting Alarm Generate DNP3 Event and Open Connection

Fleeting

(When used for the Normal state on analog and counter points)

Raise Fleeting Alarm No Action Taken

DNP3 Object Flags

Form Geo SCADA Expert Field Device
None No Action Taken No Action Taken
Log Event No Action Taken Log Flag Change Event in Data Log
Event No Action Taken Generate DNP3 event
Alarm No Action Taken Generate DNP3 Event and Open Connection

The Severity type and action settings provide up to five options. The availability of these options is defined by the Device Profile for your Field Device (see WITS Device Profiles). The descriptions of the settings (below) include the terminology that you should look for in your Device Profiles:

 

When you first configure WITS database points, you should choose the type of Severity that meets your requirements. However, you should also monitor the number of events being logged and alarms being raised. If you find that the Field Device's memory is filling too quickly, you may need to adjust the type of events being generated. Typically, you would reduce the number of events by changing the limits, hysteresis, persistence, and so on. You may also decide to poll for events more frequently. However, you may decide to stop certain events being generated, in which case you will need to set the Severity of some states/flags to None instead of Event.

 

To configure the severities and actions for a WITS database point:

  1. Log on to ViewX via a user account that has the Configure permission, and then display the Form for the point (see Display a Form).
  2. Select the <Point> tab, where <Point> is the type of point you are configuring, for example Analog Point.
  3. In the Alarm Limits or States section, there are two Severity settings, positioned in adjacent columns. Use the Severity settings in the left column to specify the severity type and action for each point limit or state. Choose None, Alarm, Fleeting, Event, or Log Event as required.
  4. In the DNP3 Object Flag Actions section, use the various combo boxes to choose the action for each flag. For more details, see DNP3 Object Flag Actions.
  5. With Analog points, there is also an Action field in the Significant Change Detection by the Outstation section. Choose None, Log Event, Event, or Alarm as required. For more information, see Specify Whether the Outstation is to Detect Significant Changes in Value.
  6. Save the configuration.

  7. When you have completed the point configuration, you will need to download it to the Field Device by using the Outstation item's Download Configuration action.

    If your Field Device does not support download configuration, you will need to make the same changes to the Field Device's configuration locally.

Further Information

Configuring a WITS Analog Point


Disclaimer

Geo SCADA Expert 2019