Source Name

Associated with: WITS Application programs.

 

The Source Name attribute shows the name of the Field Device (outstation) in which an application program is located.

You can specify the application program's outstation on the Application Program tab within the Application Program form ((see Configuring a WITS Application Program)).

Further Information

Source Name.


Disclaimer

Geo SCADA Expert 2019