TCP/IP Type for WITS Network Communications

You can use the Network tab on the WITS Outstation Form to specify the TCP/IP Type for each network connection. The protocol can be:

The TCP/IP Type for a WITS Outstation item has to match the TCP/IP Type of the DNP3 Channel(s) used to communicate with the Field Device. For more details on the TCP/IP Type setting for a Channel, see Configure a Channel's Network Connection Properties.

The Network tab has TCP/IP Type settings for outbound connections (Geo SCADA Expert to Field Device) and inbound connections (Field Device to Geo SCADA Expert).

TCP/IP Type Outbound and Inbound Network Connections

Typically, you would set the TCP/IP Type during the initial configuration of the Outstation item to match the communications configuration of the Field Device. It is unlikely that you would then make any further changes to the TCP/IP Type in Geo SCADA Expert.

If you change the TCP/IP Type in Geo SCADA Expert and then download the configuration, communications will be lost. To restore communications, you need to:

  1. Re-configure the TCP/IP Type of the other Outstations that use the same Channel(s).
  2. Re-configure the Channel(s) to have a TCP/IP Type that matches that of the Outstations.

Take care when altering the TCP/IP Type of a Channel. Changing the communications protocol for a Channel will result in loss of communications to any Outstation that uses a different protocol.

Further Information

Configure a WITS Field Device to Initiate Only

Configure a WITS Field Device to Listen Only

Configure a WITS Field Device to Listen and Initiate via the Same Connection

Configure a WITS Field Device to Listen and Initiate via Separate Connections.


Disclaimer

Geo SCADA Expert 2019