For E-mail / Voicemail Redirection use an E-Mail Action.
To successfully redirect an alarm by forwarding the details in an e-mail:
- The servers on your system have to be configured to send e-mail messages (see E-Mail Settings).
- The database items for which alarms might need redirecting have to be assigned geographical coordinates (if your system uses Geo SCADA Expert's Geographical Location features and alarms are to be redirected to users that are in the relevant geographical region)
- The users to which you want to send e-mails must have:
            - Valid e-mail accounts (see Define the E-Mail, Pager, and Voicemail Contact Settings for a User).
- WebX access if they will be using an Original WebX client when acknowledging alarms via e-mail and/or accessing the item’s Alarm View from a hyperlink embedded in the e-mail (see Define whether a User can Access the System via ViewX, WebX or Phone).
- The security permissions needed to acknowledge the alarms (see Allocating Security Permissions).
- Geographical regions within which they are 'responsible' for alarms (if alarms are to be redirected to users that are in the relevant region) (see Assign Regions of Responsibility).
- Geographical coordinates (if Geo SCADA Expert is to compare a user's geographical location with an alarm's region when determining to whom alarms should be redirected).
 
- If e-mails are to be sent to multiple users:
            - Suitable User Groups and / or User Rosters have to exist in the database (see User Groups, and see Configure a User Roster).
- Each user has to be a member of the relevant User Group (see Associate a User with a User Group).
- Each User Group and / or User Roster has to be assigned the geographical regions within which they are responsible for alarms (if alarms are to be redirected to users that are in the relevant region) (see Assign Regions of Responsibility).
- Each user in a User Group and / or User Roster has to be configured to receive the e-mails via the same E-Mail Contact number (either 1, 2, 3, or 4) (see Define the E-Mail, Pager, and Voicemail Contact Settings for a User).
 
- If users are to acknowledge alarms by entering an Acknowledgment Keyword in the subject line of the reply to the e-mail, that Acknowledgment Keyword has to be specified on your system’s servers (see E-Mail Settings).
- If users are to acknowledge alarms by deleting all, or part, of a Hiding Keyword from the body of the reply to the e-mail, that Hiding Keyword has to be specified on your system's servers (see E-Mail Settings).
Use the E-Mail Action Form’s E-Mail Action tab to define various settings, including:
- Whether the e-mail should only be sent to recipients that are logged on to the Geo SCADA Expert system
- Whether the e-mail should only be sent to users that are in the relevant geographical region (this only applies if your system uses Geo SCADA Expert's Geographical Location features)
- The recipient(s) of the e-mail
- The contact account to which to send the e-mail
- The importance of the e-mail
- The e-mail’s subject
- The e-mail’s content.
Configure each E-mail Action so that the correct engineer receives the e-mail, and the e-mail contains the relevant information. Each e-mail is customized for the individual recipient. This includes the overall format of the e-mail, which can be sent in either:
- Plain text format (see Plain Text Format E-Mails)
- HyperText Markup Language (HTML) format (see HTML Format E-Mails).
You specify the required e-mail format on each user’s User Account Form (see Define the E-Mail, Pager, and Voicemail Contact Settings for a User in the Geo SCADA Expert Guide to Security). Other properties—such as a User Account’s Locale and Date Format—further determine how an e-mail is customized for an individual recipient.
To configure an E-mail Action’s properties and message:
- Display the Action Form for the E-mail Action that you want to configure.
- Select the E-Mail Action tab.
     
- Use the Inhibit Action combo box to define under what circumstances Geo SCADA Expert should be inhibited from sending the e-mail:
            - Never—Send the e-mail to each of the chosen users, regardless of whether those users are logged on to the system.
- If actioned users are logged on—Send the e-mail to the chosen users, provided that none of the chosen users are logged on to the system from a ViewX client, Virtual ViewX client, or an Original WebX client.
- If actioned users are logged on from a WebX client—Send the e-mail to the chosen users, provided none of the chosen users are logged on to the system from an Original WebX client.
- If actioned users are logged on from a ViewX client—Send the e-mail to the chosen users, provided none of the chosen users are logged on to the system from a ViewX or Virtual ViewX client.
 
- Use the Retries field to specify the maximum number of times that Geo SCADA Expert will attempt to re-send an e-mail if the initial attempt is unsuccessful. Use this field in conjunction with the Retry Interval field (see below).
- Use the Retry Interval field to specify the duration between attempts to re-send an e-mail. Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value. For example, enter 30S for a 30-second interval.
- Use the Redirection Scheme combo box to specify whether you want to redirect alarms to users that are in the relevant region or suitable geographical location. If your system does not use Geo SCADA Expert's Geographical Location features, or you want to redirect alarms regardless of a users' region or location, select the default option 'User, Group or Roster'.For information about the other Redirection Scheme options, see Specify Whether to Redirect Alarms to Users According to Geographical Criteria. 
- The Send To field directly below the Redirection Scheme combo box only applies when the Redirection Scheme is set to the default option of 'User, Group or Roster'. (If another Redirection Scheme option is selected, the Send To field is grayed out and unavailable for use.)Use the field to specify the User, User Group, or User Roster to which Geo SCADA Expert is to redirect alarms. To do this: - Select the browse button next to the Send To field.
 A Reference browse window is displayed. 
- Use the Reference browse window to locate and select the name of the required User, User Group, or User Roster. (For further information, see User Accounts in the Geo SCADA Expert Guide to Security; see User Groups in the Geo SCADA Expert Guide to Security; or see Configure a User Roster.)
            Only users with an e-mail address are valid (see Define the E-Mail, Pager, and Voicemail Contact Settings for a User in the Geo SCADA Expert Guide to Security). 
- Select the OK button.
 The Reference browse window is closed and the selected entry is shown in the Send To field.
 
- Select the browse button next to the Send To field.
- Regardless of the option chosen for the Redirection Scheme, use the E-Mail Contact combo box to specify to which e-mail contact account the message is to be sent. (Each user can be allocated up to four e-mail addresses through which they can be contacted. Each address is allocated to a separate E-Mail Contact Account—see Define the E-Mail, Pager, and Voicemail Contact Settings for a User in the Geo SCADA Expert Guide to Security.)
    If you specified an option other than 'User, Group or Roster' as the Redirection Scheme, Geo SCADA Expert uses the E-Mail Contact Account to transmit the redirected alarm messages to the users that it identifies as suitable recipients during its region and/or location searches. WARNING MISDIRECTED ALARM NOTIFICATIONS When configuring Geo SCADA Expert to redirect alarms to a User Group or User Roster, ensure that each user account in that User Group or User Roster is configured to receive messages via the specified E-Mail Contact number (1, 2, 3, or 4).Likewise, when configuring Geo SCADA Expert to redirect alarms to Users according to geographical criteria, ensure that the user account of each user that has 'responsibility' for alarms in the relevant region is configured to receive messages via the specified E-Mail Contact number (1, 2, 3, or 4).Failure to follow these instructions can result in death, serious injury, or equipment damage.
- The Region field only applies if you specify the 'To Region Users' option for the Redirection Scheme. Use the field to specify the geographical region for which recipients of the e-mail message are to have 'alarm responsibility'. For more information, see Specify Whether to Redirect Alarms to Users According to Geographical Criteria.
- If you specified a Redirection Scheme option other than 'User, Group or Roster', use the fields in the Find in Region section to specify the users to whom Geo SCADA Expert should redirect alarms when no users are in the relevant geographical region. For information about configuring the fields in this section, see Specify Whether to Redirect Alarms to Users According to Geographical Criteria.
- Use the Importance combo box to define the priority of the e-mail. When the recipient receives the e-mail, it will display its importance—the recipient can use the importance to determine which e-mails take priority. 
        Choose from High, Normal, and Low. 
- Use the Alarm View check box to specify whether the e-mail is to include a hyperlink to the relevant Alarm View (if such a view exists for the item that is in alarm).
        Select the Alarm View check box to include a hyperlink. The format of the hyperlink varies, depending whether the e-mail is in Plain Text or HTML format (see Plain Text Format E-Mails, and see HTML Format E-Mails). For an example of each type of hyperlink, see Send an E-Mail in Different Formats to Different Users. In order to access the Alarm View using the hyperlink and display that view in a Web browser using Original WebX, the intended recipient(s) need to have WebX access (see Define whether a User can Access the System via ViewX, WebX or Phone in the Geo SCADA Expert Guide to Security). Clear the check box if no hyperlink is required. This option might be preferable, for example, for security purposes, or if the language used on your system includes characters that are not supported by hyperlinks in Plain Text e-mails (see Plain Text Format E-Mails). 
- Enter the title of the e-mail in the Subject field. The title can contain both plain text and trip sequences (see Trip Sequences Supported by Redirection Actions, and see Use Trip Sequences to Include Geographical Information). 
        Regardless of the E-Mail’s format, the Subject is sent as 7-bit US-ASCII, a character set to which limitations apply (see Plain Text Format E-Mails). 
- Select the Message field.
- Enter the e-mail message. This can include trip sequences (see Trip Sequences Supported by Redirection Actions, and see Use Trip Sequences to Include Geographical Information).
        If the e-mail is being sent to telephony software, also see E-mail / Voicemail Redirection. If any of the recipients can receive HTML format e-mails, you can include HTML tags and character entities (such as <) in the e-mail message. Any tags and character entities have to conform to the HTML 4.0 Transitional standard (see HTML Format E-Mails). If the Send Using Plain Text Only feature is activated on the recipient’s user account, the recipient will only be sent e-mails in plain text format (see Define the E-Mail, Pager, and Voicemail Contact Settings for a User in the Geo SCADA Expert Guide to Security). 
- Save the configuration.
When you have configured the required E-Mail Actions, you can proceed to Configure Alarm Redirections for an Item or Group.