Display the Action Form

You need to use the Action Form to configure the properties of each redirection action. To display the Action Form:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Right-click on the redirection action in the Database Bar.
    A context-sensitive menu is displayed.
  3. Select the Edit Properties option.
    The Action Form for the selected redirection action is displayed.

Each Action Form has these tabs:


Disclaimer

Geo SCADA Expert 2020