Enable or Disable Client Licensing

Geo SCADA Expert systems can be licensed at the ViewX client(s) or at the server. There are certain factors you should consider when deciding where to enable licensing:

Ultimately, the type of license file that is supplied by Schneider Electric determines which of the licensing methods you need to use—you can only use client licensing if you are supplied with a client license file; you can only use server licensing if you are supplied with a server license file.

To enable or disable client licensing:

  1. Display the Client Configuration Window for the connection that you want to add or edit.
  2. Either:
    • Select the Use Client Licensing check box to enable client licensing for the selected client. The client will use its own license rather than request a ‘floating license’ from the server. This option should only be used with clients that are designed to access the system continuously.

      Or:

    • Clear the Use Client Licensing check box to disable client licensing for the selected client. The client will request a ‘floating license’ from the server when it attempts to connect to the system. This option should only be used with clients that are designed to access the system occasionally.

When you have enabled or disabled client licensing for the client, you can proceed to define the other client configuration settings. However, before the client license feature can be used, you will need to associate the client with the client license file (Associate a ViewX client - System Connection with a Client License).

You can also define the Use Client Licensing setting by editing the Systems.xml file manually Use the Systems.xml File to Set Up a ViewX Client Connection.


Disclaimer

Geo SCADA Expert 2020