Failed Third-Party OPC Client - System Connections

If the third-party OPC client - system connection cannot be established, you will be unable to connect to Geo SCADA Expert from the third-party OPC client application.

The connections will fail to establish if:

The third-party OPC client - system connection works in the same way as a ViewX - system except that it uses a different license and it requires Data Access components to be installed on the OPC client PC. As such, the firewall rules for third-party OPC client - system connections are the same as those for ViewX - system connections.

Further Information

Firewall Settings for Client - System and Server Advise Connections.

Understanding Client - System and Server Advise Connections.

Certificates for Geo SCADA Expert Server and Client Connections.

Use the Server Status Tool to ascertain the current status of server - client connections: see Server Status Information.

 


Disclaimer

Geo SCADA Expert 2020