Create an EtherNet/IP Direct Outstation Set

When you create the outstation set, you can leave most of the fields at their default values. The only fields that you need to change for this tutorial are:

Save the configuration.

For further information on configuring an EtherNet/IP Direct Outstation Set, see Configure an EtherNet/IP Outstation Set.

Once you have configured the outstation set, you can proceed to Create an EtherNet/IP Direct Outstation.


Disclaimer

Geo SCADA Expert 2020