Create an EtherNet/IP Analog Point

This analog point is set up to control the plant and also to monitor value changes. When you create the analog point, you can leave most of the configuration fields at their default values.

On the Analog Point tab, the only fields that you need to change for this tutorial are:

On the Control tab, you need to set:

On the Historic tab, you need to set:

Save the configuration.

For further information on configuring an EtherNet/IP Analog Point, see Configure Analog Points.

Once you have configured the analog point, you can proceed to Create a Mimic.


Disclaimer

Geo SCADA Expert 2020