Display a Queries List
There are several ways of displaying a Queries List in Geo SCADA Expert.
On a ViewX client or a Virtual ViewX client, you can display a Queries List from:
- The Queries Bar (see Display a Queries List from the Queries Bar)
- The Database Bar (see Display a List from the Database Bar)
- Another display, such as another List or a Mimic (see Display a List from another Display).
You can also display a Queries List on an Original WebX client (see View and Action Lists on an Original WebX Client).
If Data Grids, Data Sets, or Data Tables exist on your system, you can Display the Data on a Data Grid, Data Set, or Data Table in List Format
You can Display User Query Data.
While a Queries List is displayed, you can perform any of the following to change how the information is displayed on that List: