Display the Events List for an Item or Group
            You can display an Events List that is filtered automatically to show the Events for a specific item or group. You can display such an Events List from:
- The Database Bar (see Display a List from the Database Bar)
 - From another display, such as a Mimic or another List (see Display a List from another Display).
 
In either case, use the Display Events menu option or pick action to display the required Events List. The List will be filtered automatically to include only those events for the selected item or group.
If you select a Group folder, the Events List also shows the events for the items in that folder and its sub-folders.
The Events List is pre-filtered by time—the period for which events are initially shown is defined by the Event List Range specified your User Account (or the Guest User Account if you are not logged onto the system).
Your user account settings, security permissions and so on, may further restrict the events to which you have access. This is to help ensure that you are only made aware of events that might be of interest to you.