Specify the Properties of any Grid Lines
This section applies to Lists other than Alarms Lists.
Use the Grid Lines section on the Option window’s Lists tab to specify these properties:
- Size—Use to specify the line thickness of grid lines used to separate cells on Lists other than Alarms Lists. The default is 1.
If required, either specify a different line thickness, or specify 0 for grid lines to be excluded from any Lists that are displayed on that particular ViewX client.
- Color—Use to specify the color of the grid lines that separate the cells in Lists other than Alarms Lists.
Click on the color if you want to change it. A pop-up color window is displayed. Either select a color from the window, or select the ... option and create a custom color (see Using the Color Window in the Geo SCADA Expert Guide to Core Configuration).
Example:
On a particular ViewX client, grid lines are configured as cyan: