Define the Data Coding Scheme for an SMS Service

The type and amount of characters you can use in an SMS message is dependent on the data coding scheme that is in place. Geo SCADA Expert supports two data coding schemes for SMS messages:

If you need more information about the characters supported in the data coding schemes, refer to:

When you configure an SMS Pager Service, you need to choose the appropriate type of data coding for your needs:

For information on the commands that have to be supported by your GSM modem, see SMS - Short Message Service.

To define the Data Coding Scheme for an SMS service:

  1. Display the Pager Service Form and then select the SMS Service tab.
  2. Choose the required setting from the Data Coding Scheme combo box:
    • GSM—You can use many of the characters included in the GSM 03.38 standard in your SMS messages. The maximum number of characters per message is 160.

      The characters that are included in GSM 03.38 but which cannot be used in Geo SCADA Expert SMS messages are:

      Symbol

      Description

      Ξ

      Greek Capital Xi

      No symbol

      Form Feed

      ^

      Caret

      {

      Left brace

      }

      Right brace

      \

      Reverse solidus

      [

      Left square bracket

      ~

      Tilde

      ]

      Right square bracket

      |

      Vertical sign

      Euro sign

  3. Save the configuration.

Disclaimer

Geo SCADA Expert 2020