Define the Number of Times an SMS Service will attempt to Process Messages

Each SMS Service has an Incoming SMS Fail Limit which you can configure on the SMS Service Form. This property allows you to define when Geo SCADA Expert will generate an alarm associated with an SMS service receiving invalid SMS messages.

The Incoming SMS Fail Limit works in conjunction with an internal Fail count which starts at 0 and increases by 1 each time an invalid SMS message is received. It is reset to 0 each time a valid SMS message is received or when a manual reset is triggered (see Checking and Resetting the Fail Count for an SMS Service). If the Fail count exceeds the Incoming SMS Fail Limit, an alarm is raised.

An SMS message is deemed to be invalid if:

To define the Incoming SMS Fail Limit for an SMS Service:

  1. Display the Pager Service Form.
  2. Select the SMS Service tab.
  3. Enter the Incoming SMS Fail Limit that you require. The Incoming SMS Fail Limit is set to 5 by default which is appropriate for many systems.
  4. Save the configuration.

Further Information

Define whether an SMS Service can Process Incoming Messages.

Checking the Fail Count for Incoming SMS Commands.

Checking and Resetting the Fail Count for an SMS Service.


Disclaimer

Geo SCADA Expert 2020