Define whether Geo SCADA Expert Replies to Incoming SMS Messages

When Geo SCADA Expert receives an SMS command, it processes the command, but by default, does not send a reply to the sender of the SMS message. This does not affect the running of a system, but may mean that the sender of the SMS is unable to determine whether the SMS command was successful. This is especially true if the sender is in a remote location without access to a system client.

By using the Acknowledge SMS Commands setting on the SMS Service Form, you can configure Geo SCADA Expert to reply to incoming SMS messages. This means that the sender of the message is notified of the outcome of the message being sent to Geo SCADA Expert:

If an SMS command fails or is rejected, an alarm is also raised in Geo SCADA Expert (the alarm also provides a brief description of the cause of the problem).

To configure Geo SCADA Expert to reply to incoming SMS pager messages:

  1. Display the Pager Service Form.
  2. Select the SMS Service tab.
  3. Select the Process Incoming SMS Messages check box (so that it is checked).
  4. Choose the required setting from the Acknowledge SMS Commands combo box:
  5. Save the configuration (see Saving Configuration Changes in the Geo SCADA Expert Guide to Core Configuration).

Disclaimer

Geo SCADA Expert 2020