Adding a Random Generator

To create and configure an item in the database, you need to be logged on as a user with the Configure Database feature enabled, and allocated the relevant permissions (see User Accounts).

To add a Random Generator to the database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the Group to which you want to add a new Random Generator.
  3. Select the Create New option.
    A context-sensitive menu is displayed.
  4. Select the Other option.
    A context-sensitive menu is displayed.
  5. Select Random Generator.
    A Random Generator is added to the Group. It is selected automatically, ready for you to enter its name.
  6. Give the Random Generator item a relevant name (see Naming Restrictions).

After you have added the Random Generator, display its configuration Form (see Display a Form).

 

The Random Generator Form has these tabs:

When you have finished defining the settings for the Random Generator item, Save the configuration.


Disclaimer

Geo SCADA Expert 2020