Understanding Geo SCADA Expert Security

Security is applied by the Geo SCADA Expert servers to every client that accesses the system (ViewX, Virtual ViewX, Original WebX, third-party OPC applications, and so on.). For example, a user that accesses the system via a third-party OPC client is subject to the same restrictions as when accessing the system via ViewX.

The Geo SCADA Expert security features are designed to:

Geo SCADA Expert Security

Geo SCADA Expert has three levels of security:

Overall system security

The overall security of Geo SCADA Expert is managed within the Server Configuration Tool. This tool allows you to define the default level of security for the whole system including:

User accounts

Each system user requires a user account to access the system. User accounts define the features that a user can access using ViewX and other client applications. You can either manage user accounts directly in Geo SCADA Expert, or remotely by associating them with Windows or LDAP (Lightweight Directory Access Protocol) user accounts.

Access Control List (ACL)

Each item in the database can have its own security settings that define which User accounts and User Groups can access the item, and which features are available. This is called the Access Control List (ACL) for the item. A set of permissions can be allocated to each account to define which features can be accessed by users.

Third-party applications that access Geo SCADA Expert will use a configured user account or the built-in Guest user, depending on whether client security is supported by the Third Party application (see Security for Third-Party Applications).


Disclaimer

Geo SCADA Expert 2020