Multi-Monitor and Multiple Instance Clients

In some cases, ViewX may be configured to operate as one of the following:

If this is the case, the functionality of the ViewX client may be limited due to the settings that are used to configure these types of systems. For example, the client may be configured to run in single document mode or as a restricted workstation.

Your system administrator should advise you if a client is configured to operate as a Multi-Monitor or Multiple Instance setup. They should also provide you with information about any limitations that may apply to the ViewX client based on its configuration settings.

Further Information

Launch a ViewX client on a Multi-Monitor Setup

Configure ViewX Instances to Access Different Servers

Miscellaneous Options for ViewX clients.


Disclaimer

Geo SCADA Expert 2020