Device Port for WITS Network Connections
You can use the Network tab on the WITS Outstation Form to specify the Device Ports for:
- The communications port on the Field Device that 'listens' for a connection from Geo SCADA Expert (outbound connections)
- The communications port on the Field Device that initiates a connection to Geo SCADA Expert (inbound connections).
For more details, see Device Ports for WITS Field Devices.