Health Check Status

Associated with: WITS Outstations.

 

WITS Field Devices can send health check status information to Geo SCADA Expert for the following attributes:

 

After Geo SCADA Expert has first communicated with the Field Device:

 

When the status of a health check attribute changes, Geo SCADA Expert may log the details in the Event Journal (if logging is enabled) (see Understand Events Lists in the Geo SCADA Expert Guide to Lists). Geo SCADA Expert may also raise an alarm (see Understand Alarms and see Define the Severity for Health Check Logging).


Disclaimer

Geo SCADA Expert 2020