Working with the Virtual ViewX Manager
The Virtual ViewX Manager is an application that is installed on each Virtual ViewX server machine. The application provides information about the server's communication settings, Virtual ViewX license, file locations, and so on.
This topic summarizes the information that is shown on each tab of the Server Manager window.
POTENTIAL LOSS OF COMMUNICATIONS OR SECURITY BREACH
To display the Server Manager window:
-
In Windows, select the Start menu. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder.
- Select the Virtual ViewX Manager option.
With a Virtual ViewX server installation that is activated and licensed, the Server Manager Window is displayed - see below.
(On new installations, the Product Registration Wizard is displayed - see License your Virtual ViewX Installation).
The Server Manager window contains various tabs, the contents of which are summarized below.
To close the Server Manager window, select the Close button.
Further Information