MessageOff
Description
The Off message for the tag. This property applies to discrete tags. The Off message is the message associated with the FALSE state of the discrete tag. The maximum number of characters is 64. A discrete tag set to 0 is in the FALSE state. All tags created by Geo SCADA Expert are analog tags (including digital points), and therefore this property is not applicable.
Geo SCADA Expert Metadata Field
WH_MessageOff
Default Value
The default value for this property is an empty string.
Type
String.
Further Information