MessageOn
Description
The On message for the tag. This property applies to discrete tags. The On message is the message associated with the TRUE state of the discrete tag. The maximum number of characters is 64. A discrete tag set to 1 is in the TRUE state. All tags created by Geo SCADA Expert are analog tags (including digital points), and therefore this property is not applicable.
Geo SCADA Expert Metadata Field
WH_MessageOn
Default Value
The default value for this property is an empty string.
Type
String.
Further Information