Configure the Y-Axis Label
You can specify a label for the y-axis. The label is a text string that identifies the axis. You specify the label's properties using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).
Use the Label section of the window to specify the properties associated with the axis label:
- Label: Enter a suitable label for the axis or use the browse button and select a tag from the database (Geo SCADA Expert will use the value of the tag as the label for the axis). If you enter a label directly in the field, remember that the text has to be enclosed within single straight quotation marks ' '. For information on using property tags, see Property Tags in the Geo SCADA Expert Guide to Expressions.
Leave the Label field empty if no axis label is required.
- Color: Use the Color button to specify the required color. You can select a color from the Color Palette or select the ... option to display the Color window. You can use the Color window to create a custom color (see Using the Color Window in the Geo SCADA Expert Guide to Core Configuration).
- Position: Use the combo box to specify the position of the axis label.