File Upload Forms have several ‘tabs’ for configuring different aspects of File Upload information. For drivers that support File Uploading, a combination of these tabs is available:
Use to optionally define a Help View and to indicate whether the File Upload is to be excluded from any Exclusive Control activity (see Defining Identification Details).
Use to specify the item's geographical coordinates. (You need only configure the properties on this tab if your system uses Geo SCADA Expert's Geographical Location features.)
Use to define any custom pick actions (‘methods’) for the File Upload (see Using the User Methods Tab to Define Custom Actions).
Use to define optional features associated with any File Upload alarms (see Defining an Item or Group’s Alarm Properties).
Use to define any alarm redirections for the File Upload (see Configure Alarm Redirections for an Item or Group).
Use to Specify the File Upload Settings.
This section explains the features on the File Upload and Historic tabs that are common to File Uploads on several drivers.
For aspects of File Upload configuration that are common to most types of database item, see the Geo SCADA Expert Guide to Core Configuration.
For aspects of File Upload configuration that are specific to individual drivers, see the Geo SCADA Expert driver-specific documentation.