Configure the Advanced Trio Diagnostic Properties that are Specific to Analog Points

Use the fields on the Analog Point tab to configure the analog input point properties and output point properties that are specific to the Advanced Trio Diagnostics driver. Some of the fields are common to many Advanced Trio Diagnostics points (see Configure the Common Point Properties). Fields that are specific to Advanced Trio Diagnostics Analog Input points and Advanced Trio Diagnostics Analog Output points are explained below.

Further Information

Persistence: see Use Persistence to Stop Fleeting Changes in Value from Changing a Point State.

The other properties on the Analog Point tab that are not shown in the above figure are common to analog points on many drivers. For information on the fields, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2021