Defining Analog Point Details

Use Analog Points within the Geo SCADA Expert database to represent measuring instruments or control devices that can be in any of a range of values. The raw input values received from the plant are scaled into engineering values or floating-point values, that the server can process. You then define the full range of values in which an analog point can reside, by using the Full Scale and Zero Scale limits on the Point Form. You use other state limits to represent the point when its value is within specific ranges. You can specify a suitable description for each of these states, and define whether an event is logged, or an alarm is raised upon entry into each state.

You configure each analog point on your system by using the fields on the appropriate Analog Point Form. Each Form has several tabs, which you use to define different aspects of the point configuration.

Use this section, along with the appropriate driver documentation, for information on configuring the analog points on your system.

This section explains how to configure analog point properties that are common to many analog points. Most of these properties are displayed on the Analog Point tab of the Analog Point Form (on some advanced drivers, these properties are displayed on a separate tab).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

If the point is an analog output point:

If the point in an internal analog point, you need to use the Manual tab to:

(In addition to internal analog points, Geo SCADA Expert also supports Variables. The type of database item that you add to Geo SCADA Expert depends on that item’s intended functionality. For more information, see Variables in the Geo SCADA Expert Guide to Core Configuration.)

In circumstances where the server uses separate alarm limits to the outstation, those limits are configured on the Master Station Alarm Limits tab of the Analog Point Form (see Master Station Alarm Limits).

 


Disclaimer

Geo SCADA Expert 2021