Redirect Alarms to Users that are Responsible for a Particular Region Regardless of Location

Although the examples in this topic apply to systems that use Geo SCADA Expert's Geographical Location features, some of the principles and configuration properties described also apply to systems that do not use Geographical Location features.

The example in this topic demonstrates how you might configure Geo SCADA Expert to redirect alarms only to users that have 'responsibility' for a particular geographical region. This type of redirection configuration is:

 

On a particular system, the users are expected to be static (based at a particular site, rather than move from one site to another). User database items are used to represent the users in the Geo SCADA Expert database. The User database items are stored in a Group in the database.

The system extends across several geographical regions. Each region is represented by a Region item in the database. Different users are 'responsible' for different regions. Each User is assigned to one or more User Groups in the database (do not confuse User Groups with the 'object' Groups that are used to define the hierarchy in which items are stored in the database). The Regions tab on each User Group is used to define the region(s) for which the users in that particular User Group are 'responsible'. (Alternatively, or in addition, a user can be assigned User Groups on the Regions tab of the User Form, or of any User Rosters with which the User account is associated.)

Suitable database items are configured in the Geo SCADA Expert database to represent the plant.

The Group in which the plant database items are placed is configured to redirect the plant's alarms by e-mail. This requirement is configured on the Redirection tab of the Group's configuration Form. The tab references the E-Mail Action database item that is used to specify the e-mail criteria. (If the alarms were to be redirected by pager or SMS message, you would use a Pager Action instead. Likewise, if the alarms were to be redirected using a third-party alarm redirection application - such as a voice alarm announcement system - you would use a Method Action (User) redirection action instead.)

On the E-Mail Action tab of the E-Mail Action's configuration Form, the Redirection Scheme is specified as 'To Region Users', and the relevant region specified in the Region field.

Whenever an alarm is raised for part of the plant, Geo SCADA Expert checks whether the alarm matches the redirection criteria on the relevant plant Group's Redirection tab. If so, it then checks whether the alarm matches the criteria of the E-Mail Action that is listed on that tab. If the criteria are met, Geo SCADA Expert redirects the alarm to those users that are 'responsible' for the region that is specified on the E-Mail Action's Form.

In the case of plant that is in the 'NE Plant Group', the alarms are redirected to users that are responsible for alarms in the 'North-East' region. This includes the users that are in the User Group named 'System Engineers - North', as the Responsible Regions field for that User Group includes that region.


Disclaimer

Geo SCADA Expert 2021