When filtering an Alarms List or Alarm Banner by Source, you can include wildcard characters in the filter criteria. Wildcard characters allow a single character to match any of one or more unspecified characters. The Sources filter on the Alarms List or Alarm Banner’s Filter window supports these wildcard characters:
- ? (question mark) matches a single character.
			Example: N? Region.Water Level 
 will match Sources such as NE Region.Water Level and NW Region.Water Level
- * (asterisk) matches any number of characters.
					Example: *Pager* 
 will match any Sources that include the string ‘Pager’.
- # (hash) matches any single digit (0 to 9).
					
					Example: Zone #.Sensor # 
 will match Sources such as Zone 1.Sensor 2, Zone 1. Sensor 3, and Zone 2.Sensor 4.
- [ ] a case-sensitive list, enclosed in square brackets. A Source is included if it starts with any one of the characters or digits that are specified in the list.
					Example: [abc]* 
 will match any Sources that start with the lowercase letters a, b, or c. It will not match any Sources that start with uppercase A, B, or C.[a,b,c]* 
 will match any Sources that start with a lower-case comma or the lowercase letters a, b, or c. This is because the comma is recognized as a valid character in the same way as a letter. Again, it will not match any Sources that start with an uppercase comma, A, B or C.[a-f]* 
 will match any Sources that start with a lowercase letter in the range a to f inclusive[f-a]* 
 will match any Sources that start with a lowercase letter f or a. Ranges are only recognized if the characters are defined in alphabetical order. As the first character defined is f and this comes after a in the alphabet, there is not a valid range.[A-FM-PST]* 
 will match any Sources that start with an uppercase letter in the ranges A to F, or M to P, or either uppercase S or uppercase T.
- [!] a case-sensitive list, enclosed in square brackets, with the first entry prefixed with an exclamation mark. A Source is excluded if it starts with any one of the characters or digits that are specified in the list.
					Example: [!abc]* 
 will exclude any Sources that start with the lowercase letters a, b, or c. It will not exclude Sources that begin with uppercase A, B or C.
Further Information
Pre-filter alarms by Alarm Source using the Alarm Filter String: see Specify a Default Alarm Filter.
(The filter wildcards that are supported by Lists other than the Alarms List differ to the above—for information, see Filter Wildcards in the Geo SCADA Expert Guide to Lists.)