When the Is Like or Is Not Like Filter Condition Types are used to filter a List such as an Events List, 
- _ (underscore) matches any single character.
            
            For example CA_ will match CAT, CAN, CAB, but will not match CATCH, CALL or CA. 
- % (percent) matches any number of characters.
            
            For example CA% will match CAT, CAN. CAB, CATCH, CALL or CA. 
To include a wildcard character in a search without causing the wildcard to match other characters, enter a backslash (\) before the wildcard character. For example PUMP\_1 will only match PUMP_1, and will not match PUMP11, or PUMPA1.
Further Information
The filter wildcards that are supported by Alarms Lists and Alarm Banner differ to the above—for information, see Filter Wildcards in the Geo SCADA Expert Guide to Alarms.