Return to Normal Alarm

Digital points and some types of analog and counter-type points support the ability to raise an alarm when the point's value returns to that point's normal operating state or range of values. With analog and counter-type points, the alarm comprises a fleeting alarm. This feature can be useful if you want users to be made aware of when a point has returned to its normal state, or you want to use that alarm notification for other functions, for example in Logic programs, or to trigger or cancel alarm redirections. Be aware, however, that configuring such points to raise an alarm when their values return to the normal operating state or range of values (known as raising a 'Return to Normal' alarm) could potentially impact your operators' ability to distinguish between alarm notifications that indicate an abnormal occurrence, and that of a 'Return to Normal' alarm. This is because both types of alarm trigger the types of activity you expect when an alarm is raised (see Activities that Occur when an Alarm is Raised). For example, by default the alarms appear in the Alarm Banner and Alarms List, and the relevant animated objects on Mimics change to show that an alarm has been raised. Likewise, the point's Status display shows that the point is in an alarm state, however with a 'Return to Normal' alarm, the Status display also indicates that the point is in its normal operating state.

We recommend that you only configure points to raise an alarm when their values return to the normal operating state or range of values if such a notification is specifically required on your system.

If you do use this feature, consider whether to configure 'Return to Normal' alarms in such a way as to clearly distinguish them from other types of alarm. For example, by creating and using a Severity level specifically for such alarms, and configuring that Severity level to use different colors to other alarms on your system. This will enable users to clearly distinguish between alarm notifications that indicate an abnormal occurrence, and those of a 'Return to Normal' alarm. You define Severity levels using the Geo SCADA Expert Server Configuration Tool (see Alarm and Event Severities).

If you use a different Severity specifically for 'Return to Normal' alarms, consider whether to apply an Alarm Filter to the User accounts of those users that do not need notifying of 'Return to Normal' alarms. By configuring the filter to omit alarms of that particular severity, 'Return to Normal' alarms that are assigned that severity would be omitted from Alarms Lists and the Alarm Banner while that user is logged on. For information about configuring alarm filters, see Define the Default Alarm Filter Settings for a User. For an example that demonstrates the use of a custom Severity level specifically for 'Return to Normal' alarms, see the Area of Interest example, below.

If the Area of Interest feature is enabled on your system, you might want to consider using the feature in such a way that only the relevant users are made aware of 'Return to Normal' alarms. As with other state-related alarms and events, you can specify the Area of Interest with which a point's Normal state alarms or events are associated. With such configuration, users will only be aware of the alarms and events to which they are allocated Area(s) of Interest. For more information, see Restrict Alarm and Event Access to Specific Areas of Interest. For an example that demonstrates how you might configure a different Area of Interest for alarms that are associated with a point's Normal state, see Use Multiple Point State Alarms in Conjunction with Areas of Interest (the example is specific to points that are configured to have Multiple Point State Alarms).

 

As with other alarms, 'Return to Normal' alarms are affected by other configuration, including (if applicable to the points', or your system's configuration):


Disclaimer

Geo SCADA Expert 2021