Activities that Occur when an Alarm is Raised

When an abnormal condition is detected, Geo SCADA Expert typically raises an alarm. When an alarm is raised:

When an alarm is raised, decide what action you need to take to have the cause of the alarm investigated and the abnormal condition rectified (see Perform an Action on an Alarm). If configured for the item or the Group in which it is located, you can also use the Display Alarm View option to display the ‘file object’ that is associated with the item’s alarm state.


Disclaimer

Geo SCADA Expert 2021