Alarm Banner

The Alarm Banner is the primary alarm display and is displayed at the bottom of the ViewX client window by default. The Alarm Banner can be configured to appear in one or more Window containers.

The Alarm Banner comprises the Alarm Bell Button and the Alarm Banner List.

The Alarm Banner List provides information about alarms in the same manner as the Alarms Lists. The Alarm Banner List displays alarm information using a series of columns (see Understand the Information that is Displayed on an Alarms List or Alarm Banner). Your user account settings, security permissions and so on, might restrict the alarm entries to which you have access. This is to help ensure that you are only made aware of alarms that might be of interest to you.

By default, the entries in the Alarm Banner List are ordered by State, Severity, and then Time. This results in the most recently raised Unacknowledged Uncleared alarms of the highest severity appearing at the top of the Alarm Banner. This is followed by any Unacknowledged Uncleared alarms of the next highest severity, again in chronological order. Following on from Unacknowledged Uncleared alarms are any Unacknowledged Cleared alarms in severity and then time order, and then finally any Acknowledged Uncleared alarms in severity and then time order. The alarm entries are also colored to indicate their Alarm Status.

If you select (highlight) an alarm in the Alarm Banner, Geo SCADA Expert will attempt to retain the selected alarm’s position relative to the Alarm Banner’s visible display area, regardless of other alarm activity. As such, if you select a visible alarm in an Alarm Banner that is only large enough to show a few alarms at once, the selected alarm will remain on display regardless of the number of other alarms that are raised or cleared while that alarm remains selected.

As with Alarms Lists, you can right-click on an entry in the Alarm Banner List to display a context-sensitive menu.

The figure below shows the context-sensitive menu for an entry in the Alarm Banner in ViewX:

(The menu options that are available for an alarm entry vary, depending on your user account settings, the selected item's configuration and security settings, and so on.)

You can select an option from the menu to:

If Alarm Banner scripts are used on your system, additional ‘custom’ options may be available from the Alarm Banner’s context-sensitive menu. These might include 'custom' menu options that provide access to regularly-used Alarm Banner filters. See a system administrator for the documentation associated with such custom actions.

If your User Account is configured to allow you to select multiple alarms in ViewX and you display the context-sensitive menu while more than one alarm is selected, a subset of menu options is shown.

The Alarm Banner is hidden by default on a Virtual ViewX client (providing that your User Account enables you to hide the Alarm Banner (see Define which Alarm Banner and Alarms List Features are Available to a User in ViewX and Virtual ViewX)). This is by design, to provide more display space for viewing other Geo SCADA Expert displays, such as Mimics, Trends, and Queries Lists. (You can display the Alarm Banner by selecting the Alarm Banner command from the ViewX ribbon.)

Further Information

Specify the Preferred Alarm Banner and Alarms List Options on a ViewX Client.

Use Alarm Banner scripts to optionally add ‘custom’ actions to the Alarm Banner’s context-sensitive menu on a ViewX client: see Alarm Banner Scripts.

Display the Alarm Banner in 'Fill' Container mode on a Multi-Monitor Setup: see Launch the Alarm Banner in Fill Container Mode.


Disclaimer

Geo SCADA Expert 2021