Adjust the Columns on an Alarms List or the Alarm Banner
Alarms Lists and the Alarm Banner display these columns by default:
| Order and Names of Columns | Width of Alarm Banner Column on a ViewX Client | Width of Alarms List Column on a ViewX Client | Width of Alarms List Column on a Virtual ViewX Client |
|---|---|---|---|
| Severity |
82 |
80 |
75 |
| Time |
282 |
160 |
150 |
| Source |
301 |
312 |
350 |
| Message |
444 |
275 |
450 |
| Category |
200 |
183 |
100 |
| System |
200 |
200 |
--- |
| Area of Interest |
200 |
198 |
200 |
| Suppressed Alarm Count |
200 |
200 |
200 |
The Area of Interest column is only displayed if the Area of Interest feature is enabled on your system (see Restrict Alarm and Event Access to Specific Areas of Interest).
If you are working with multiple databases on a ViewX client you should ensure that the Area of Interest feature is configured the same way for all systems.
The System column is only displayed on a ViewX client that is configured to access Multiple Databases.
You can use the Alarm Columns window to adjust the columns that are displayed on an Alarms List or the Alarm Banner (see Use the Alarm Columns Window to Change the Alarms List or Alarm Banner Columns). You can use the window to:
- Change the column order
- Resize a column
- Hide a column.
If the Allow Column Resizing check box is selected on the Alarms and Events tab of the Options window (see Specify the Preferred Alarm Banner and Alarms List Options on a ViewX Client), you can also:
- Change the Order of Columns on an Alarms List or the Alarm Banner Directly.
- Change the Size of Columns on an Alarms List or the Alarm Banner Directly.
Users with the required permission can add additional columns to the Alarms Lists and Alarm Banner, if required (see Configure Additional Alarm Columns).
The Alarm Banner is hidden by default on a Virtual ViewX client (providing that your User Account enables you to hide the Alarm Banner