ViewX Client

ViewX is a feature-rich Windows application designed to provide you with day-to-day access to your Geo SCADA Expert system. A PC that uses ViewX to connect to Geo SCADA Expert is referred to a ViewX client.

Typically,a Geo SCADA Expert system contains a central Geo SCADA Expert server and multiple ViewX clients. The ViewX clients present users with information from the Geo SCADA Expert database and also send user-defined actions to the Geo SCADA Expert server.

By logging on a ViewX client, you can interact with remote devices via the Geo SCADA Expert server. For example, you could use a ViewX client to issue a control to a device - the control is sent from the ViewX client to the Geo SCADA Expert server, where it is processed and sent to the appropriate device. The Geo SCADA Expert server then updates the database to indicate the outcome of the control attempt.

You can use a ViewX client to perform a wide range of tasks on your Geo SCADA Expert system, including issuing controls, responding to alarms, and configuring the database. However, your user permissions may restrict access to features depending on your duties. For example, operator-level users are often able to use ViewX to monitor a system and respond to alarms, but are denied access to configuration features.

When you log on to a ViewX client, you access the Geo SCADA Expert system via a ViewX window.

As an operator, you will predominantly use ViewX to access:

Similar displays can also be accessed from a Virtual ViewX client.

On either client, the functions are accessed via drop-down menus, the ViewX ribbon, or context sensitive menus that can be selected with the mouse. You can also use keyboard shortcuts to access many of the features.

For information on using a ViewX client, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021