System-Wide Alarm and Alarms List Preferences

This section summarizes those Alarm and Alarms List options that a system administrator can configure on a system-wide basis. Such options, if required to differ from the defaults, should be specified on each server when a Geo SCADA Expert system is first installed. The options are specified using the Geo SCADA Expert Server Configuration Tool.

You can use the Geo SCADA Expert Server Configuration Tool to:

To access a Geo SCADA Expert system, users typically log on via a User Account. Anyone who accesses the system without logging on, is logged on automatically via the Guest or Web User accounts.

Use the Root or System Group Form to define the system-wide settings for the Guest User, including:

  • Whether the Allow Group Alarm Operations feature is made available to the Guest User.
  • The Default Alarm Filter that defines the alarms to which the Guest User has access.
  • If the Area of Interest feature is used on your system, any Area of Interest Filters. This can also affect which alarms are visible to the Guest User.

For information on configuring any of the above, see Define the Global Settings for All Guest and Web User Accounts.

If required, the ability to acknowledge specific alarms can optionally be restricted to a particular User, User Group, or ViewX workstation. Such a restriction is configured on a per-item or per-Group basis. For information, see Set Responsibility Action.

You can optionally use Alarm Banner scripts to add ‘custom’ actions to the Alarm Banner’s context-sensitive menu (see Alarm Banner Scripts).


Disclaimer

Geo SCADA Expert 2021