Decide When Geo SCADA Expert is to Execute a System Command

Geo SCADA Expert can trigger a system command under various circumstances. You need to decide when Geo SCADA Expert is to execute each system command, in order to determine the type of configuration that you need to undertake:

In addition to the above, Geo SCADA Expert is supplied with a built-in command line tool, to enable third-party applications to run Geo SCADA Expert commands from the Windows® command prompt. For more information, see Server Command Line Tool in the Geo SCADA Expert Guide to Server Administration.


Disclaimer

Geo SCADA Expert 2021