Server Command Line Tool

You can use the built-in Geo SCADA Expert Server Command Line Tool to run commands from the Windows command prompt. This can be useful if you need to access the Geo SCADA Expert server commands from other programs or via remote access that limits you to using command lines. For example, you may want to run Geo SCADA Expert server commands within batch files for third-party software applications.

If the Geo SCADA Expert server is configured to only communicate with clients that provide valid client certificates, you have to run the Server Command Line Tool on the server itself. A server requires the clients to have certificates if its Require Client Certificates check box is enabled in the Connection Security section of the Server Configuration Tool (see Configure the Connection Security Settings).

With the topics in this section, we explain how to:


Disclaimer

Geo SCADA Expert 2021