Configure the Connection Security Settings

You use the Connection Security section of the Geo SCADA Expert Server Configuration Tool to set up the server's certificate settings for communications with the other servers and clients on your system. The Connection Security section is located within the System Configuration branch of the tool. We strongly recommend that you set up your system to use trusted certificates to initiate secure connections and encrypt the data that is transmitted between the Geo SCADA Expert servers and clients. For more information about the use of certificates and also about the configuration settings that are required for client certificates, see Certificates for Geo SCADA Expert Server and Client Connections.

You use the Connection Security section of the Geo SCADA Expert Server Configuration Tool to configure these settings:

Server Certificates

You use the properties in this section to specify whether the server uses certificates for communications with other servers and clients, and if so, which certificates are used.

On systems on which server certificates are used, the Geo SCADA Expert server provides its certificate to the clients, so that the clients can verify that the server is a valid Geo SCADA Expert server. The client will decline the connection if the server does not have a valid certificate (or has no certificate at all) (see Certificates for Geo SCADA Expert Server and Client Connections). The exception to this is clients that are running a version of Geo SCADA Expert that is earlier than Geo SCADA Expert 2020. Such clients use a different communications protocol and are exempt from requesting valid server certificates.

WARNING

inability to synchronize databases and take over as main

With Geo SCADA Expert 2020 onwards, take care to ensure that Main and Standby servers all have compatible Connection Security configuration and valid certificates. We recommend that you renew certificates well in advance of their expiry dates. If the Main server is unable to connect to a Standby server due to differences in TLS (Transport Layer Security) configuration, then the Standby server will appear to attempt to synchronize endlessly with the Main server. Should a changeover occur in this situation, the Standby server will not be able to become Main. This is because it will have an invalid database due to the synchronization not having completed.
Failure to follow these instructions can result in death, serious injury, or equipment damage. If a changeover occurs with no Standby available to take over as Main, the system will be offline until a server with a valid database is brought back online.

If a Standby server is unable to connect to the Main server due to a TLS configuration conflict, the Server Icon on the Standby server will go magenta to indicate that an issue has been detected. The Server icon's context-sensitive menu will indicate that there is Invalid Standby Configuration and the dialog box will provide further information about the issue (see The Server Icon). If this is due to a TLS configuration conflict, you should check both sets of Connection Security settings on both servers and ensure that there are no issues with the certificates that either server is using. For example, a conflict will occur if the Standby server is configured to validate partner certificates, but is not able to do so because the Main server is using a temporary certificate. Do not perform any manual changeovers until the TLS configuration conflict has been resolved.

If the Main server goes offline before the Standby server has been able to complete the synchronization process, that Standby server will not be able to take over as Main. If no other Standby servers exist or have fully synchronized databases and a changeover occurs, this could result in the system going offline. To bring the system back online, restart the server that was Main. If that is not possible, contact Schneider Electric for assistance. You might be advised to restore the database on one of the servers that has an invalid database, using the most up-to-date backup in order to minimize data loss. Following this, ensure that all of the servers have compatible Connection Security configuration to enable successful synchronization to occur, and that any other issues that might be preventing synchronization have been resolved (see Check that Standby Servers are Synchronized with the Main Server).

Client Certificates

You use the properties in this section to specify whether the server is only to communicate with clients that provide valid client certificates, and if so, to specify various settings for those certificates. (If client certificates are used, you also need to set up the required client connection security for each client (see Configure the Client Connection Security Settings in the Geo SCADA ExpertGuide to Client Administration).)

On systems on which client certificates are used, each client is required to provide a valid certificate to the server, so that the server can verify that the client is a valid client. The connection request is declined if the client does not have a valid certificate (or has no certificate at all) (see Certificates for Geo SCADA Expert Server and Client Connections). The exception to this is clients that are running a version of Geo SCADA Expert that is earlier than Geo SCADA Expert 2020. Such clients use a different communications protocol and are exempt from requiring valid client certificates.

WARNING

potential security breach

Clients that are running a version of Geo SCADA Expert that is earlier than Geo SCADA Expert 2020 use a different communications protocol and are exempt from requiring valid client certificates. We recommend that you upgrade all of your clients as soon as it is practicable, to ensure that they run a version of Geo SCADA Expert that does support client certificates.
Failure to follow these instructions can result in death, serious injury, or equipment damage. The breach in system security could expose sensitive data and leave the database vulnerable to unauthorized and potentially malicious use.

Legacy Protocol

With the Allow clients/partners to use legacy protocol check box in this section, either:

Apply the changes to the server.
The changes take effect immediately.

Remember to make similar configuration changes to any other servers in your system.

Further Information

Understand the information that is displayed in the Server Certificates field: see Add a Certificate to the Server Certificates List.

Configure the Connection Security settings that apply to outgoing server-to-server connections when this server connects to another server as a client: see Connection Security Tab (for Server-to-Server Communications).

Configure the Connection Security settings on client machines: Configure the Client Connection Security Settings in the Geo SCADA Expert Guide to Client Administration.


Disclaimer

Geo SCADA Expert 2021